Technical FAQs

Ask a Question

What is suffix 5305?

Issue:
What is suffix 5305?

Product Line:
QO and QOB

Environment:
Circuit Breakers

Cause:

Resolution:
The suffix 5305 contains a special construction of a high magnetic calibration of 17 times, and also has ring tongue terminals.  10-30 amps only.
Was this helpful?
What can we do to improve the information ?