Technical FAQs

Ask a Question

What is the suffix for terminal nut kit on bottom side? What is suffix TA or TB on Powerpact ILINE construction?

Product Line:
Powerpact H, J. L, M and P frame circuit breaker

Environment:
ILINE construction

Resolution:
ILINE shroud and jaws are on the top side the breaker

-TA indicates English terminal nuts on the OFF end instead of lugs.
-TB indicates Metric terminal nuts on the OFF end instead of lugs.

Example part number:   HGA36100TA
Part numbers with this suffix are most likely not profiled, so you will want to build this part number in "product selector".
This suffix also valid for Powerpact M and P frame.
Please refer to your local Square D- Schneider Electric distributor or sales office for further help.
Was this helpful?
What can we do to improve the information ?