Technical FAQs

Ask a Question

What is the maximum size of main that can be used with the CQO116M100RB100?

Issue:
Application

Product Line:
CQO Load Centre

Environment:
Main breaker

Cause:
Maximum size of main breaker allowed

Resolution:
The CQO116M100RB100 is labeled as 125A maximum mains.
Was this helpful?
What can we do to improve the information ?