Technical FAQs

Ask a Question

Can you power up the the ATV61 and ATV71 drive in the lab and program the drive before going to the job site?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
They want to program the drive in the lab and want to know if the drive will hold the program until they get to the job site.

Resolution:
Yes, you can power up the drive in the lab and program it before going to the job site. You will need to know how the drive is going to be controled and will need the Motor data information to be able to set up the drive before going to the job site.
Was this helpful?
What can we do to improve the information ?