Technical FAQs

Ask a Question

What is the operating temperature range for NEMA rated lighting contactors?

Issue:
What is the operating temperature range for NEMA rated lighting contactors?

Product Line:
NEMA lighting contactors

Environment:
Applies to class 8903, type S and L(X)

Cause:
Customer wants to know if he requires a heater for cold environment

Resolution:
The operating range for Class 8903 Type S and Type L(X) is 0 - 40 degrees Centigrade.
Was this helpful?
What can we do to improve the information ?