Technical FAQs

Ask a Question

What is a "U" suffix on a breaker, such as QBP32250U?

PRODUCT LINE
Powerpact Q frame Circuit Breakers

RESOLUTION
The QBP32250U is an internal part number and cannot be ordered. If can appear on a breaker label only by a plant error.  The actual breaker part number should be on the nameplate
Was this helpful?
What can we do to improve the information ?