Technical FAQs

Ask a Question

Can a PKGTAB be used with a PK15GTAL?

Issue:
Compatibility

Product Line:
Load Center Accessories

Environment:
Ground bar accessories

Cause:
Selection

Resolution:
No, they are not compatible. The PKGTAB was designed for use with the PKxxGTA ground bars, but not the PKxxGTAL ground bars. Due to the extra thickness of the busbar used in the PKxxGTAL kits, the mounting screws to mount the ground bar to the PKGTAB are too short.
Was this helpful?
What can we do to improve the information ?