Technical FAQs

Ask a Question

Was the obsolete QO40MP suitable for use with either copper or aluminum wire?

Issue:
Product feature

Product Line:
Obsolete QO Load Center

Environment:
Fusible Pullout Main

Cause:
Clarification

Resolution:
Yes, either copper or aluminum wire was acceptable.
Was this helpful?
What can we do to improve the information ?