Technical FAQs

Ask a Question

What is the adjustable magnetic (instantaneous) trip setting of the LA, LH, LC and LI breakers?

Product Line:
Circuit Breaker types LA, LAL, LH, LHL, LC, LCL, LI, and LIL
 
Resolution:
Circuit Breaker types LA, LAL, LH, LHL, LC, LCL, LI, and LIL include a feature that allows field adjustment of the instantaneous trip value (magnetic trip). The attached file shows those values. Note that there is a difference in the Series 1 and Series 3 LC and LI breakers. Also note that the Low and High Trip Value may vary from -20% to +25%.  
 
Breaker Type: LA, LH, LAL, LHL
Breaker Amp Rating AC Adjustable Magnetic Trip
Low * High *
125 625 1250
150 750 1500
175 875 1750
200 1000 2000
225 1125 2250
250 1250 2500
300 1500 3000
350 1750 3500
400 2000 4000
 
Breaker Type: LC, LI, LCL, LIL (Series 3)
Breaker Amp Rating AC Adjustable Magnetic Trip
Low * High *
300 1500 3200
350 1750 3200
400 2000 3200
450 2250 4200
500 2500 4200
600 3000 4200
 
Breaker Type: LC, LI, LCL, LIL (Series 1)
Breaker Amp Rating AC Adjustable Magnetic Trip
Low * High *
300 1500 3000
350 1750 3500
400 2000 4000
450 2250 4500
500 2500 5000
600 3000 5400

* Low and High Trip Value may vary from -20% to +25%

Note:  the long-time pickup for these thermal-magnetic breakers is NOT ADJUSTABLE.  
Was this helpful?
What can we do to improve the information ?