Technical FAQs

Ask a Question

Is the Canadian Load Center Catalog number QO8L100RB Service Entrance Rated?

Issue:
Load Center Ratings 

Product Line:
Canadian QO Load centers

Environment:
Load Center Application 

Cause:
Service Entrance Rating

Resolution:
The Canadian Electric Code requires load centers for Service Entrance Applications to be a Main Breaker, to have the bonding screw factory installed and a Service Barrier that restricts any load wiring to exit or enter the Service Area(or top endwall) of the load center. So the QO8L100RB is NOT Service Entrance Rated.
Was this helpful?
What can we do to improve the information ?