Technical FAQs

Ask a Question

Do we offer a 30 mm flashing LED pilot light?

 

Issue:
Do we offer a 30 mm flashing LED pilot light



Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause:
Do we offer a 30 mm flashing LED pilot light

 
Resolution:
We only offer a flashing LED pilot light in the 22 mm line of operators.

For 30 mm operators we do have a flashing (not LED) light module for 110-120V 50/60HZ part number 9001KMF1.

For 22 mm operators we have flashing modules at 24VAC/VDC part number: ZBV18B*, 110-120VAC part number: ZBV18G*, and 230-240VAC part number ZBV18M*. The * will be filled in with a number determining color where 1 is white, 3 is green, 4 is red, 5 is orange, and 6 is blue.

 
 
Was this helpful?
What can we do to improve the information ?