Technical FAQs

Ask a Question

Do we have replacements for the obsolete shockproof contactors?

 

Issue: Do we have replacements for the obsolete shockproof contactors?


Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause: Shockproof contactors

 
Resolution: For new installations up to 38 amps the Tesys U or Tesys D with DC coils are available. The Tesys U meets new requirements and are the choice of the French Navy; the Tesys D with DC coils and the diode bridge interface also meet new requirements, the Tesys D contactors with AC coils do not meet the new requirements.

For 40 to 95 amp we do not have contactors that completely meet the new requirements.
 

Keywords: Shockproof, tesys U, Tesys D, DC, diode bridge interface

 


 
Was this helpful?
What can we do to improve the information ?