Technical FAQs

Ask a Question

How is a damper control circuit set up on an open type ATV312, ATV61, ATV71, ATV12, etc... drive?

Issue:
How is a damper control circuit set up on an open type ATV312, ATV61, ATV71, ATV12, etc... drive?

Product Line:
Altivar open type ATV drives

Environment:
All

Cause:
The drive should not run until the damper is open.

Resolution:
The end customer's run signal can control the damper solenoid.  Once the damper is open, a sensor or limit switch can indicate an open damper status.  This damper end switch should give a contact closure to the RUN logic input on the VFD.

Note that the ATV212 and ATV61 have damper control functions integral to the standard product.
Was this helpful?
What can we do to improve the information ?