Technical FAQs

Ask a Question

Is PowerSuite compatible with the ATV71 Plus?

Issue:
Compatibility of PowerSuite and ATV71 Plus

Product Line:
ATV71 Plus

Environment:
All models and serial numbers

Cause:
None

Resolution:
In principal yes, but since mid 2012 PowerSuite is replaced by SoMove and therefore not anymore supported.
On drives up to size 15 (ATV61HC63N4 / ATV71HC50N4 / ATV71HC630Y / ATV71HC80Y) there is no
difference between ATV and ATV Plus.

Was this helpful?
What can we do to improve the information ?