Technical FAQs

Ask a Question

Is the QO11428UX200FTRB available?

Issue:
Selection

Product Line:
QO Load Center

Environment:
Kohler Generator Panel

Cause:
Availability

Resolution:
This catalog number, although offered in Digests 174 (2007), 175 (2009) and 176 (2012), was never released for manufacturing. Considering using QO11428MX200FTRB instead. The QO11428MX200FTRB would have a factory installed 200A main breaker.
Was this helpful?
What can we do to improve the information ?