Technical FAQs

Ask a Question

Is a generator interlock kit offered for the QONQ42LS400?

Issue:
Selection

Product Line:
QO Load Center

Environment:
400A Load Center

Cause:
Product availability

Resolution:
A generator interlock kit is not available for the 400A load centers. Generator interlock kits are only available for load centers rated up to 225A maximum.
Was this helpful?
What can we do to improve the information ?