Technical FAQs

Ask a Question

What Generator Interlock Kit can be used with the HOM2040L125PRB load center?

Issue:
Selection

Product Line:
Homeline

Environment:
Accessory selection

Cause:
Selection

Resolution:
Use HOMCRBGK1. Since the HOM2040L125PRB is a main lugs load center, it would need to be converted to a main breaker load center before the HOMCRBGK1 could be used. 
Was this helpful?
What can we do to improve the information ?