Technical FAQs

Ask a Question

Why does the Enclosed ATS48 not come with power fuses?

Issue:
Why does the Enclosed ATS48 not come with power fuses?

Product Line:
Enclosed ATS48

Environment:
Models with fusible disconnect

Cause:
There is no power fuses in the Enclosed ATS48.

Resolution:
Units supplied with fusible switch disconnects require the user to supply and install the power fuses based on the power circuit and load.
All of the Enclosed 48 controllers accept either UL Class J or L fuses, depending on the full load current rating.
Was this helpful?
What can we do to improve the information ?