Technical FAQs

Ask a Question

Are the ATV61/71 R1 and R2 relays mounted inside the control terminal board or the main control board?

Issue:
Are the ATV61/71 R1 and R2 relays mounted inside the control terminal board or the main control board?

Product Line:
Altivar ATV61 and ATV71

Environment:
All 

Cause:
Needs to replace the R1 and R2 relays on the ATV61 drive.

Resolution:
The R1 and R2 relays are mounted inside the control terminal POD not the main control board. 
However, the Control Terminal board is not available as a spare part but is included in the Control Board Kit, so a replacement Control board will have to be ordered, even if the control terminal board is all that gets replaced.
Was this helpful?
What can we do to improve the information ?