Technical FAQs

Ask a Question

Are there lug kits available for the NS1600 breaker, like NPNFE36160U32R?

Issue:
Are there lug kits available for the NS1600 breaker, like NPNFE36160U32R?

Product Line:
Compact NS1600

Environment:

Cause:

Resolution:
No.  The compact NS1600 like NPNFE36160U32R and NPHFE36160U32R are bus connected only, since there is not room for large enough cable to supply 1600 amps to this breaker.  Lug kits are available for 1250 amps and below.
Was this helpful?
What can we do to improve the information ?