Technical FAQs

Ask a Question

Can Conext SW have output voltage and frequency changes like XW can?

Conext SW cannot have have output voltage changes, only frequency (50/60Hz), which can be accomplished thru SCP, or XW Config 3.0 (not Pro), 
or CnxtCfgToolAI. 
Was this helpful?
What can we do to improve the information ?