Technical FAQs

Ask a Question

Is a surface cover available for the QO142M200PC?

Issue:
Availability

Product Line:
QO Load Center

Environment:
Surface cover

Cause:
Selection for application

Resolution:
This load center is provided with a combination (flush) cover that could be used for either a flush or surface installation. If a true surface cover is needed, the QOC42US could be ordered separately.
Was this helpful?
What can we do to improve the information ?