Technical FAQs

Ask a Question

What is the part number for a 3 position selector switch for an 8903 type LX lighting contactor?

Issue:
What is the part number for a 3 position selector switch for an 8903 type LX lighting contactor?

Product Line:
8903 type LX lighting contactors

Environment:
US Product Lines

Cause:
The 176 Digest lists 2 part number for a 3 position selector switch

Resolution:
To order the 3 position selector switch you will need to order the mounting bracket – 9999BLX, and the selector switch – 9999SC2.

To install the 3 position selector switch, your contactor must have a two-wire control relay – CA2SK11* (Form R6), and the mounting bracket - 9999RLX.

*add the appropriate voltage code to complete the part number

Was this helpful?
What can we do to improve the information ?