Technical FAQs

Ask a Question

Which metrics will be displayed when using the Conext Battery Monitor?

Issue:
Which metrics will be displayed when using the Conext Battery Monitor?

Product Line:
Conext Battery Monitor

Environment:
Any Schneider Electric solar installation

Cause:
Specific metrics aren't outlined on website

Resolution:
The following metrics will be displayed when using the Conext Battery Monitor:

Battery Current
Battery Temperature
Battery State of Charge
Battery Midpoint 1 Voltage
Battery Midpoint 2 Voltage
Battery Capacity Remaining
Battery Capacity Removed

You can find this and other specifications for the device on our website:
http://solar.schneider-electric.com/product/conext-battery-monitor/
Was this helpful?
What can we do to improve the information ?