Technical FAQs

Ask a Question

Can the Main breaker load center catalog number CQO160M200C be converted to a Main lugs only load center?

Product Features
Product Line:
QO Load centers
The CQO160M200C can be converted to a Main Lugs ONLY load center and requires the removal of the Service Entrance Barrier and the Neutral Bonding Screw. SEE the instruction label applied to the Service Entrance Barrier within the load center. 

Use main lug kit catalog number QOL225.

NOTE: The Canadian CODE requires the Bonding Screw to be factory installed ONLY, on Main Breaker Service Entrance rated load centers, so once the bonding screw is removed it CANNOT be
re-installed and the load center CANNOT be used as Service Entrance.

Was this helpful?
What can we do to improve the information ?