Technical FAQs

Ask a Question

Is the manual starter connected before or after the ATS48?

Issue:
Is the manual starter connection before or after the ATS48?

Product Line:
ATS48

Environment:
 All

Cause:
Installation / Setup

Resolution:
It is recommended to be installed before the ATS48 not after.

Was this helpful?
What can we do to improve the information ?