Technical FAQs

Ask a Question

Do the 8538SBA combination starters come standard with a hand-off-auto selector switch?

Issue:
Do the 8538SBA combination starters come standard with a hand-off-auto selector switch?

Product Line:
8538 Type Combination Starters

Environment:
US Product Lines

Cause:
The 176 Digest does not specify

Resolution:
No. In order to get a standard hand-off-auto selector switch, you will need to add the factory modification form 'C' to the catalog number.
Was this helpful?
What can we do to improve the information ?