Technical FAQs

Ask a Question

Wire range for 8910DPA63

Issue:
What is the acceptable wire size range that can be used with the 8910DPA63

Product Line:
8910DPA63

Environment:
US Product

Cause:
The wire size range is not published in the Digest

Resolution:
AWG14-4
 
Was this helpful?
What can we do to improve the information ?