Technical FAQs

Ask a Question

Can I order a NEMA 4X starter enclosure without conduit hole in the bottom?

Issue:
Are NEMA 4X starter enclosures available without a conduit hole in the bottom?

Product Line:
Class 9991, Class 8536, 8538, 8736, 8738, NEMA 4/4X Enclosures

Environment:
US Product Lines

Cause:
The 176 Digest does not specify

Resolution:
No. We only offer NEMA 4/4X enclosures with a conduit hole in the bottom.
Was this helpful?
What can we do to improve the information ?