Technical FAQs

Ask a Question

Can I replace the load side fuse base(s) for 8940 Type SSG combination starters?

Issue:
What is the part number to replace the load side fuse base(s) for an 8940 Type SSG combination starter?

Product Line:
8940 Type SSG Combination Starters

Environment:
US Product Lines

Cause:
The 176 Digest does not specify

Resolution:
The 8940 Type SSG load side fuse base is part number 40512-276-50*.

*This is only ONE fuse base
Was this helpful?
What can we do to improve the information ?