Technical FAQs

Ask a Question

Is the QO2125BNF, QO2125BNS or QO2125BNRB circuit breaker enclosure CSA Certified or cUL Listed?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Standards

Cause:
Clarification of standards met.

Resolution:
These QO circuit breaker enclosures are UL Listed only.
Was this helpful?
What can we do to improve the information ?