Technical FAQs

Ask a Question

Are the catalog numbers QO327M100RB and QO112M100RB both CSA and UL Listed?

Issue:
Product Features

Product Line:
QO load centers 

Environment: 
load center listings

Cause: 
Application and location usage

Resolution: 
No, the QO327M100RB and QO112M100RB are ONLY UL listed, they are NOT CSA listed. For CSA Listed load center catalog numbers, see the Canadian Digest.

 
Was this helpful?
What can we do to improve the information ?