Technical FAQs

Ask a Question

What is the maximum short circuit current rating for the QO3100BNF, QO3100BNS or QO3100BNRB circuit breaker enclosure?

Issue:
Application

Product Line:
Circuit breaker enclosure

Environment:
Application

Cause:
Clarification

Resolution:
The maximum short circuit current rating for these circuit breaker enclosure is 22,000A.
Was this helpful?
What can we do to improve the information ?