Technical FAQs

Ask a Question

What is the catalog number for the replacement rod of 9422TF Operating mechanism?

Issue:
What is the catalog number for the replacement rod of 9422TF Operating mechanism?

Product Line:
Operating Mechanism

Environment:
Applies to 9422 ARC, BN, BP, RC, ARD, RD, ARN, RN, ARP, RP, ATC, TC, ATD, TD, ATCF, TCF, ATCN, TCN, ATDF, TDF, ATDN, TDN, ATEF, TEF, ATEN, TEN, ARE, BR, RE, ARF, RF, ARR, RR, ART, RT, ATF, TF, RX

Cause:
Customer wants replacement Rod for this disconnect

Resolution:
9422R1 is the replacement rod 15.5" long
 

One is required for all the following: 9422 ARC, BN, BP, RC, ARD, RD, ARN, RN, ARP, RP, ATC, TC, ATD, TD, ATCF, TCF, ATCN, TCN, ATDF, TDF, ATDN, TDN, ATEF, TEF, ATEN, TEN

Two are required for all the following: 9422 ARE, BR, RE, ARF, RF, ARR, RR, ART, RT, ATF, TF, RX
(one rod is used to operate the device and the second is used as a stiffener rod)

Was this helpful?
What can we do to improve the information ?