Technical FAQs

Ask a Question

Lever arm selection for L100/L300

Issue:
How does one pick out a lever arm for an L100/L300 limit switch?

Product Line:
Type A roller arms for L100/L300 limit switches

Environment:
US Product

Cause:
L100/L300 product selection is different than other limit switches

Resolution:
For an arm with a 0.25" wide, 0.75" diameter steel wheel, pick based on length:

AC - 1.25"
AA - 1.50"
AD - 1.75"
AH - 2.00"
AJ - 2.25"
AO - 2.50"
AK - 2.75"
AB - 3.00"
AL - 3.50"
AM - 4.00"
AN - 4.50"
AP - 5.00"
AQ - 5.50"
AR - 6.00"


To modify the roller, use the following suffix(es):

1 - 1" diameter roller
4 - 1.25" diameter roller
2 - 1.50" diameter roller
N - Nylon roller
R - Ball bearing roller (0.75" diameter)
NS - Stainless steel roller pin, nylon roller

Was this helpful?
What can we do to improve the information ?