Technical FAQs

Ask a Question

What is the part number for the main breaker barrier used on the CQO140M200C, Series S05 Load Center?

Issue:
Repair parts

Product Line:
CQO Load Center

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The barrier is part number 40559-262-01. The label attached to the barrier is part number 40270-516-01.
Was this helpful?
What can we do to improve the information ?