Technical FAQs

Ask a Question

XW MPPT80 Aux port typo

XW MPPT80 Installation Guide  975-0540-01-01 (Rev.B) has conflicting descriptions of Aux port pinouts on pgs. 2-10 (correct) and 2-16 (incorrect).
XW MPPT80 Installation Guide  975-0540-01-01 (Rev.E) has incorrect assignment of NO and NC connections for fan circuit (should be COM and NO). 
See attached.
Was this helpful?
What can we do to improve the information ?