Technical FAQs

Ask a Question

Are crimp lugs available for the QMB367MW?

Issue:
Alternate lugs

Product Line:
QMB

Resolution:
Yes, either (3) VCEL-050-12H1 (500 KCMIL) or (3) VCEL-075-12H1 (750 KCMIL) could be used, per phase. Order lugs separately from Schneider Electric or Hubbell Power Systems, Inc.
Was this helpful?
What can we do to improve the information ?