Technical FAQs

Ask a Question

Maximum Auxiliary contacts on 8702 reversing contactor

Issue:

What is the maximum number of auxiliary contacts that can be added to each side of an 8702 reversing contactor?

Product Line:

8702SB, 8702SC, 8702SD 2 and 3 pole reversing contactors

Environment:

US product

Cause:

There are a different number of auxiliary contacts that can be added to contactor depending on the size

Resolution:

Up to 4 contacts can be added to each side of a 2 or 3 pole, size 0, 1, or 2 reversing contactor.  The first two contacts will attach to the contactor viathe supplied mounting bracket.  The two additional contacts will attach to the first two contacts with a 6-32 1" screw, no 6 star lock washer, and 6-32 hex nut.  If all four contacts are to be used, one return spring from the contactor must be removed.  See the instruction sheet supplied with th contacts for instructions.
 

Was this helpful?
What can we do to improve the information ?