Technical FAQs

Ask a Question

Why is my XW going into a charge cycle while selling?

The Recharge Volts setting will trigger a new BULK charge. If customer is using another brand of charge controller, the Grid Support Volts 
setting will need to be set lower than the float voltage for the charge controller. Especially if the XW has old firmware, the battery voltage may drop up to 2V 
lower than the Grid Support Voltage before it exits Grid Support mode. If the Recharge Volts is set too closely to Recharge Volts, it may trigger nuisance 
charge cycles, especially in cold weather (temp compensation). Upgrade to the latest firmware and make sure to have at least 2V difference between Grid Support 
Volts and Recharge Volts for a 24V system, and 4V difference for a 48V system.
Was this helpful?
What can we do to improve the information ?