Technical FAQs

Ask a Question

What is required to field install a 150VA control transformer in an enclosed D-Line unit?

Issue:
What is required to field install a 150VA control transformer in an enclosed D-Line unit?

Product Line:
TeSys Enclosed D-Line

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
To field install a control transformer, you will need an insta-kit: LA9TFD15*


*add the appropriate voltage code to complete the part number
Was this helpful?
What can we do to improve the information ?