Technical FAQs

Ask a Question

Will LDB wireway connect to Hoffman wireway?

Issue:
Compatibility with Hoffman NEMA 1 wireway
 
Product Line:
General Purpose Wireway
 
Environment:
LDB
 
Cause:
Installation
 
Resolution:
 
 
 
 
Yes, it will connect and both lines are ANSI49 color.
Was this helpful?
What can we do to improve the information ?