Technical FAQs

Ask a Question

Can I use XW+NA Aux port to auto start my generator?

The XW+NA aux port can be used to drive an external 12VDC relay provided the coil draws <250mA. This relay (not supplied) will work with a 2-wire generator 
start to trigger on low voltage and clear at a higher voltage (user settable). If the generator does not have it's own cool down circuitry, it would be better to incorporate 
the XW AGS (865-1060-01) so the gen is allowed a cool down period to run unloaded for a time before stopping. 
Was this helpful?
What can we do to improve the information ?