Technical FAQs

Ask a Question

What size of breaker to use with the SDSA1175?

Issue:
What size of breaker to use with the SDSA1175?

Product Line:
Surge protection devices

Environment:
Applies to the SDSA1175

Cause:
Instruction bulletin does not say the recommended size of the breaker to be used with the SDSA1175

Resolution:
The leads of the SDSA1175 are recommended to be connected to a 2-pole 15-30A breaker
Was this helpful?
What can we do to improve the information ?