Technical FAQs

Ask a Question

Lox L100/L300 rod type lever arm

Issue:
What is the part number for a rod type lever arm for a L100 or L300 limit switch?

Product Line:
L100/L300 RB Denison Lox Switches

Environment:
US Product

Cause:
There is no part number listed in the Digest for this

Resolution:
The part number is simply R.  The R rod holder accepts round rods with a diameter of 0.187"

 

Was this helpful?
What can we do to improve the information ?