Technical FAQs

Ask a Question

What is part number 30072-007-67?

Issue:
What part is a 30072-007-67

Product Line:
8536S starters

Environment:
US Product

Cause:
Customers occasionally provide this as a part number to distributors

Resolution:
This is the part number for a warning label inside of a size 0 or size 1 NEMA starter.  It is not the part number of a starter itself.

 

 
Was this helpful?
What can we do to improve the information ?