Technical FAQs

Ask a Question

What are the rating plugs for the Micrologic Series 4 PE circuit breaker like PEF2036LIG?

Issue:
What are the rating plugs for the Micrologic Series 4 PE circuit breaker like PEF2536LIG?

Product Line:
Micrologic Series 4 breakers

Resolution:
The available rating plugs for this series of breaker are below. Because these are becoming obsolete, check for availability.
 
Circuit Breaker Frame Size Ampere Rating   Cat. No.
Micrologic PE Series 4 1200 A 600 A
700 A
1000 A
1200 A
PE120600RP PE120700RP PE121000RP PE121200RP
1600 A 1000 A
1200 A
PE161000RP PE161200RP
2000 A 1000 A
1200 A
1400 A
1600 A
1800 A
PE201000RP PE201200RP PE201400RP PE201600RP
PE201800RP
Was this helpful?
What can we do to improve the information ?