Technical FAQs

Ask a Question

What is the second 0 in the Form H300?

Issue:
What is the second 0 in the Form H300?

Product Line:
Class 9065 Solid State Overloads

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The extra 0 indicates that the solid state overload is sized down from it's standard amp range to a range of 6-18 amps.
Was this helpful?
What can we do to improve the information ?