Technical FAQs

Ask a Question

Does Schneider Electric offer a 600 Ampere double throw switch in Type 4 stainless steel?

Issue:
Product Feature

Product Line:
Double Throw Safety Switch

Environment:
600A, Type 4

Cause:
Request for quote

Resolution:
Our double throw safety switches are offered in stainless steel enclosures through 400 Ampere maximum.
Was this helpful?
What can we do to improve the information ?