Technical FAQs

Ask a Question

XW AGS Gen Warmup

The XW AC2 transfer delay can be adjusted using XW Config or Combox. This allows for gen warmup in cold areas. 
This parameter is in the INVERTER, not the AGS. See attached.
Was this helpful?
What can we do to improve the information ?